Certifications
Lapp Muller SAS improves its performances, so qualitative as economic, by protecting the environmental frame during its production activities.
LONG-LASTING IMPROVMENT
Since several years, Lapp Muller SAS has been implementing a general politics of quality. Consequently, Lapp Muller SAS obtained its first certification ISO 9001 in 1996. Now it is in accordance with ISO 9001/V2008, what reflects the efficiency of the manufacturing process of our special electric cables, and also our competences, expertise and fame.
Quality is, for Lapp Muller SAS, a permanent concern in order to anticipate the requirements of our customers and to innovate constantly.
ENVIRONNEMENT
Always feeling concerned by the respect of the environmental norms, Lapp Muller SAS is ISO 14001/V2004 approved since 2008.
ROHS
All our products manufactured in LAPP Muller are RoHS compliant according to European directive 2002/95/EC-76/769/EWG and its amendment n°14 (2003/11/EG) since May 1st 2005.
HOMOLOGATION
Homologation UL
Homologation INTERBUS
Homologations DCN
On request, we can have our products certified according to well known national or international standards such as:
Bureau Veritas
Bureau Det Norske Veritas
ABS Europe LTD
Lloyds
Download the document