Customised solutions

customised-solutions-header

LAPP Muller Solutions Department: A Pionneer of Innovation

In the dynamic world of technology and engineering, the Special Technical Solutions Department stands as a beacon of innovation. Tasked with transforming standard cables into ready-to-run complete system solutions, from producing high-tech cables to developing sophisticated over-moldings and connectors, the team's expertise spans across various specialized workshops. These include the machine workshop, plastic workshop, and connector and equipment workshops, all of which are integral to the department's operations.

 

When in house production becomes an added value

While the trend is to rely on outsourcing, we take the opposite approach. This strategy gives us complete control over our projects, ensuring reliability and accountability. We do not depend on external parties who might withdraw in times of difficulty, which is especially important in fully customized projects where many unexpected problems can arise.

 

The Department's Core Operations

At the heart of the Solutions department's success lies its unique approach to problem-solving. We not only design and produce equipment in-house, but also integrate multiple components into seamless solutions. This includes high-risk operations such as the mounting of hybrid and optical connectors, which require precision and care due to their fragile nature.

One of our notable achievements in collaboration with the special projects department is the development of fiber optic cables used for communication. These equipped cables, designed for defense and other critical sectors, are meticulously crafted and tested to ensure reliability and performance in extreme conditions. The process involves machining, plastic over-molding, and precise connector mounting, demonstrating the department's comprehensive capabilities. 

 

Meeting the Demand for 360° Solutions

In today's fast-paced and technologically advanced world, many customers are seeking single suppliers that can provide a complete 360° solution. They don't just need a cable; they need an entire intelligent system that integrates seamlessly into their operations.  By offering a comprehensive suite of services – from initial concept development to final product implementation – we ensure that our clients receive a fully integrated solution tailored to their specific requirements. This holistic approach sets us apart in the industry and allows us to deliver exceptional value to our customers.

 

Examples of our Devised Solutions

Robotic Application
Heavy Anchoring System with Hybrid Cable
Deep Sea Anchoring System
Anchoring Systems
3D printed Moldings for plasturgicaly operations
Spiral Cables
Optical Subsea Connections
Optical Subsea Connections
Coaxial Cable Reel
Embedded Systems
Cable solutions for harsh environment

Success Story: Groundwater Monitoring and Protection Project

Groundwater Monitoring

Customers Problem: A Moroccan client, actively serving coastal cities in Morocco, was facing a significant issue with their drinking water sources becoming contaminated with seawater. This problem arose due to excessive groundwater pumping, leading to the intrusion of seawater into freshwater aquifers.

Our Proposed Solution: The department developed a specialized cable system equipped with sensors to monitor the dielectric behavior of groundwater. This system could detect changes in water composition, signaling when freshwater was being contaminated by seawater. The solution involved creating an over-molded cable with 60 conductors, each connected to sensors strategically placed to measure water quality changes.

Result: The implementation of this innovative solution allowed for real-time monitoring of groundwater quality. The Moroccan client could now receive alerts when their water sources were at risk of contamination, enabling them to take proactive measures. The system proved successful, ensuring a sustainable and safe drinking water supply for several cities in Morocco and even extending its benefits to cities in France, such as Nice and Montpellier. This project has significantly contributed to the protection of precious freshwater resources


    We are always available to answer your questions. Please do not hesitate to contact us directly: